How to get Maximum Supply Currents

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to get Maximum Supply Currents

跳至解决方案
2,122 次查看
ko-hey
Senior Contributor II

Hi all

As for the "Table 14. Maximum Supply Currents" in IMX6SXCEC.

It's not mentioned about how to get a value.

I found a calculation formula for i.MX6Q from following thread in i.MX community.

About max supply current in i.MX6Q.

The formula is as follow.

--------------------------------------------------

General equation for estimated, maximum power consumption of an IO power supply:

Imax = N x C x V x (0.5 x F)

Where:

N—Number of IO pins supplied by the power line

C—Equivalent external capacitive load

V—IO voltage

(0.5 xF)—Data change rate. Up to 0.5 of the clock rate (F)

In this equation, Imax is in Amps, C in Farads, V in Volts, and F in Hertz.

--------------------------------------------------

Is the formula appropriate to i.MX6SoloX ?

Ko-hey

标签 (3)
0 项奖励
回复
1 解答
1,957 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right: this formula is applicable to i.MX6SX too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,958 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

you are right: this formula is applicable to i.MX6SX too.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,957 次查看
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

I understand.

Ko-hey

0 项奖励
回复