How to format eMMC using U-boot in imx6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to format eMMC using U-boot in imx6?

4,585件の閲覧回数
hishamelmeligi
Contributor II

I am working on a custom board with imx6. I am trying to use the fastboot on the eMMC to flash the MBR table but it works only if the eMMC has gpt format. 

How to partition the eMMC for the first time if it is mounted on the board already.

0 件の賞賛
返信
1 返信

2,915件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Hisham

please refer to programming emmc with uboot (Warp7 board)

http://git.denx.de/?p=u-boot.git;a=blob;f=board/warp7/README;h=60339da543732829d4ac09f02178cb84dfa3b...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信