How to format eMMC using U-boot in imx6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to format eMMC using U-boot in imx6?

3,947 次查看
hishamelmeligi
Contributor II

I am working on a custom board with imx6. I am trying to use the fastboot on the eMMC to flash the MBR table but it works only if the eMMC has gpt format. 

How to partition the eMMC for the first time if it is mounted on the board already.

0 项奖励
回复
1 回复

2,277 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hisham

please refer to programming emmc with uboot (Warp7 board)

http://git.denx.de/?p=u-boot.git;a=blob;f=board/warp7/README;h=60339da543732829d4ac09f02178cb84dfa3b...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复