How to force enable SYNC signal on ESAI0 bus at boot time (in probe)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to force enable SYNC signal on ESAI0 bus at boot time (in probe)

652件の閲覧回数
samRocknrolla
Contributor I

I have an A2B transmitter (AD2428) , that connected to ESAI0 on imx8qm.

I need an enabled SYNC signal in ESAI0 for setup A2B via I2C at boot time (probe function of AD24XX driver). 

I looking SYNC signal on oscilloscope when imx8 sending audio data. But at boot time I have no correct configuration of TDM and can't start audio transferring.

Question.

Is it possible to force enable SYNC on ESAI0 at boot time ?

I can set correct frequency of ESAI0 bus in fsl_esai_dai_probe(...)

static int fsl_esai_dai_probe(struct snd_soc_dai *dai)
{
 * * *
    fsl_esai_set_dai_sysclk(dai, ESAI_HCKT_EXTAL, 49152000, 1);
 * * *
}

But misunderstand how to enable output SYNCK pin before TDM configuration.

 

 

0 件の賞賛
返信
1 返信

632件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

There are no examples on our BSP to keep SYNC signal on ESAI at boot time but, it seems that you should modify the next registers to enable it:

Transmit Control Register (TCR)
Transmit Clock Control Register (TCCR)
Receive Control Register (RCR)
Receive Clock Control Register (RCCR)

Best regards.

0 件の賞賛
返信