How to flash Images to eMMC using MfgTool2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash Images to eMMC using MfgTool2?

1,454件の閲覧回数
byunggukchoi
Contributor II

I'm trying to flash bootloader, kernel and rootfs into eMMC on IMX8MQ EVK with MFGTool2.

When running mfgtool2-yocto-mx8-evk-emmc1.vbs after downloading 4.9.88_2.0.0_mfg-tool_MX8MQ.tar.gz from NXP website, MFGTool2 returns the following error.

"Boot" body="BootStrap" error, file="C:\mfgtools\Profiles\linux\OS Firmware\firmware\imx-boot-imx8mqevk-sd.bin-flash_evk""

The settings of cfg.ini is default as described in "i.MX_Linux_User's_Guide.pdf".

The document says the default settings is for i.MX6 SoloX.

Then how to change the settings to flash eMMC on IMX8MQ EVK?

And I find that there is a directory named as "mfgtools\Profiles\Linux\OS Firmware\files\android".

But "linux" directory does not exist. I have built the yocto source code for linux version.

What should I modify to flash linux images into eMMC?

And any other information to flash images into eMMC using MfgTool2 will be helpful.

Thanks in advance.

ラベル(3)
0 件の賞賛
返信
1 返信

944件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

 Look at the following:

mfgtool imx8mq evk fails 

  Also, please check if  USB-UART driver of Silicon Labs is installed on the host PC.

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信