How to fix the camera timeout error ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix the camera timeout error ?

15,066 Views
billyhe
Contributor II

hardware environment: CPU: i.MX53, camera: OV5640

purpose: use the video for linux(v4l2) interface to get the picture with 2592x1944

dirver files: ov5640_camera.ko  mxc_v4l2_capture.ko

test program: mxc_v4l2_capture.out

add device file normal, at the end will creat /dev/video0 file

root@freescale /$modprobe ov5640_camera

root@freescale /$modprobe mxc_v4l2_capture.out

m=0, rf=30, size = 640*480 …pass

root@freescale /unit_tests$ ./mxc_v4l2_capture.out 00.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 640x480

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

  1. buf.index 1
  2. buf.index 2
  3. buf.index 0

mxc_v4l_close: release resource

m=1, rf=30, size = 320*240 …pass

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -m 1 01.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 320x240

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

  1. buf.index 1
  2. buf.index 2
  3. buf.index 0

mxc_v4l_close: release resource

m=2, rf=30, size = 720x480 …pass

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -m 2 02.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 720x480

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

  1. buf.index 1
  2. buf.index 2
  3. buf.index 0

mxc_v4l_close: release resource

m=3, rf=30, size = 720x576 …pass

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -m 3 03.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 720x576

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

  1. buf.index 1
  2. buf.index 2
  3. buf.index 0

mxc_v4l_close: release resource

m=4, rf=30, size = 1280x720 … fail, mxc_v4l_dqueue timeout

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -fr 30 -m 4 04.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 1280x720

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00100000

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

VIDIOC_QBUF failed

mxc_ipu mxc_ipu: warning: disable ipu dma channel 20 during its busy state

mxc_v4l_close: release resource

m=5, fr=15, size = 1920x1080 … fail, mxc_v4l_dqueue timeout

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -fr 15 -m 5 05.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 1920x1080

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00100000

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

VIDIOC_QBUF failed

mxc_ipu mxc_ipu: warning: disable ipu dma channel 20 during its busy state

mxc_v4l_close: release resource

m=6, fr=15, size = 2592x1944 …fail, mxc_v4l_dqueue timeout

root@freescale /unit_tests$ ./mxc_v4l2_capture.out -fr 15 -m 6 06.jpg

in_width = 176, in_height = 144   device name is Mxc Camera

out_width = 176, out_height = 144

top = 0, left = 0

sensor chip is ov5640_camera

sensor frame size is 2592x1944

sensor frame format is YUYV

         Width = 176     Height = 144    Image size = 3YUV4208016

         pixelformat = 842093913

mxc_ipu mxc_ipu: IDMAC20's EBA0 is not 8-byte aligned

mxc_ipu mxc_ipu: IDMAC20's EBA1 is not 8-byte aligned

ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

VIDIOC_DQBUF failed.

ERROR: v4l2 capture: VIDIOC_QBUF: buffer already queued

VIDIOC_QBUF failed

mxc_v4l_close: release resource

Why the picture size bigger than 720x576 will happen timeout error ? How to fix it?

Labels (2)
0 Kudos
Reply
11 Replies

9,284 Views
daiane_angolini
NXP Employee
NXP Employee

I have never used "big" capture mode to make "small" movies. So, I´m not sure it would be supported.

You need to make sure you´re using a correct configuration set to control your camera. Take a look on your camera driver and see if the frame rate are supported for a capture mode, and what would be the standard width x height.

In addition, imx53 can encode up to 720p, it won´t encode 2592x1944.

0 Kudos
Reply

9,284 Views
billyhe
Contributor II

I just want to take the photos, then I need to preview. So I use the capture mode. Do you has the better method to take photos?

Thank you very much !

0 Kudos
Reply

9,284 Views
daiane_angolini
NXP Employee
NXP Employee

As I remember ./mxc_v4l2_capture.out does not take photos. It make movies.

And, it would be better to determinate width and height of it. Something like:

./mxc_v4l2_capture.out -m 4 -h 640 -w 480


Please, see usage in order to make sure you have a correct command line.

0 Kudos
Reply

9,284 Views
billyhe
Contributor II

./mxc_v4l2_capture.out -m 4 -h 640 -w 480

If the command line just like you say, then about the ov5640, the mode 4 , width = 1280, height = 720, it's the 720P, i.MX53 can encode up to it. And your command should like this:

./mxc_v4l2_capture.out -m 4 -ow 640 -oh 480

Excute the command, it's correct. But if I excute following command:

./mxc_v4l2_capture.out -m 4 -ow 1280 -oh 720

It will happend the error like front what I said. I didn't modify the drivers ov5640 or mxc_v4l2_capture. I used the bsp was L2.6.35_11.09.01_ER_source that it is download from freescale.com.

0 Kudos
Reply

9,284 Views
daiane_angolini
NXP Employee
NXP Employee

hum. Maybe you need to take care of frame rate as well.

Sorry, I don´t have a board over here to test, and i don´t remember the complete usage for this unit-test. But, unit-test is a very-very simple, and maybe it only work great for some parameter range.

In addition, take a look on this file:

linux-2.6-imx.git - Freescale i.MX Linux Tree

Here you can see all supported capture modes:

enum ov5642_mode {
ov5642_mode_MIN = 0,
ov5642_mode_VGA_640_480 = 0,
ov5642_mode_QVGA_320_240 = 1,
ov5642_mode_NTSC_720_480 = 2,
ov5642_mode_PAL_720_576 = 3,
ov5642_mode_720P_1280_720 = 4,
ov5642_mode_1080P_1920_1080 = 5,
ov5642_mode_QSXGA_2592_1944 = 6,
ov5642_mode_QCIF_176_144 = 7,
ov5642_mode_MAX = 7

};



If you look for "720P" you will see that there is only one table definition to configure camera with 1280_720 resolution and 30 FPS.


So, if you try to use capture mode = 4 and 15 FPS, camera will not work.



9,284 Views
billyhe
Contributor II

Yes, if I use capture mode = 4 and 15 fps, camera will not work. But the demo default is 30 fps, so if I did not set it, it can be 30fps. So the camera shoud be work, but it cannot.

Pass freescale FAE's help, to change the input channel can take the bigger pictures, unfortunately, the colors has lost. And I have no idea to fix it.

Can anyone help me ?

0 Kudos
Reply

9,284 Views
shanmugamsundar
Contributor IV

hi billyhe,

        can you able to capture low resolutions such as 240p, 480p. If it so you can able to ccapture 720p also.

can you conform me whether you are using default driver file or customised one.

thanks,

shan

0 Kudos
Reply

9,284 Views
billyhe
Contributor II

Hi shanmugamsundar,

    Yes, I can capture the picture less than or equal to 1080P, and I use the default driver with ov5640.

Thanks.

0 Kudos
Reply

9,285 Views
shanmugamsundar
Contributor IV

ok now tell me your issues and what you want to do b'coz i am working on the same platform i.mx535 and ov5640. i've come across the issues what ever you are facing. i hope i can help you

Thanks

shan

0 Kudos
Reply

9,285 Views
billyhe
Contributor II

Thank you very much! Now I used the unit test to capture the picture. The command like this

./mxc_v4l2_capture.out -m 6 -fr 15 -i 1 -iw 2560 -ih 1920 -ow 2560 -oh 1920 -c 20 2592.yuv

then I used the mxc_v4l2_output.out to play the .yuv file, but it is non-distinct image.

If the mode is 5(1080P), it is no problem.

0 Kudos
Reply

9,285 Views
yangthomas
Contributor II

my mistake,

720p and 1080p are not work, esle is ok.

./mxc_v4l2_capture -iw 640 -ih 480 -ow 640 -oh 480 -m 0 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 vga.yuv

./mxc_v4l2_capture -iw 320 -ih 240 -ow 320 -oh 240 -m 1 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 320240.yuv

./mxc_v4l2_capture -iw 720 -ih 480 -ow 720 -oh 480 -m 2 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 720480.yuv

./mxc_v4l2_capture -iw 720 -ih 576 -ow 720 -oh 576 -m 3 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 720576.yuv

./mxc_v4l2_capture -iw 1280 -ih 720 -ow 1280 -oh 720 -m 4 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 720p.yuv

./mxc_v4l2_capture -iw 1920 -ih 1080 -ow 1920 -oh 1080 -m 5 -i 1 -r 0 -c 5 -fr 30 -d /dev/video0 1080p.yuv

./mxc_v4l2_capture -iw 2592 -ih 1944 -ow 2592 -oh 1944 -m 6 -i 1 -r 0 -c 5 -fr 15 -d /dev/video0 2592.yuv

if i==0

I can capture the picture less than or equal to 720*576.

0 Kudos
Reply