How to fix the Garbled problem when open the google-chrome in wayland?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to fix the Garbled problem when open the google-chrome in wayland?

2,582件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm using Linux+QT wayland as my OS system.

I'm trying to fix the problem that will appear when I open google-chrome.

It will show garbled words out like following picture.

S__21504003.jpg

How can I solve this problem?

Thanks in Advanced!

ラベル(5)
0 件の賞賛
返信
3 返答(返信)

2,454件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Wang

regarding chrome support, please refer to sect.5.6.6 Chromium Browser attached Yocto Guide:

The Yocto Project community has chromium-imx recipes to enable hardware acceleration for X11, XWayland and Wayland
version Chromium Browser for i.MX SoC with GPU hardware. Note that NXP does not support or test the patches from
community, either for VPU or GPU support.

So this can be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,454件の閲覧回数
wangvictor
Contributor III

Do I have to mail my question to this place "meta-freescale-owner@yoctoproject.org" ?

0 件の賞賛
返信

2,454件の閲覧回数
wangvictor
Contributor III

Sorry for asking this question.

How to use this Mailing List?

0 件の賞賛
返信