How to fix DDR bus width with i.MX6DL-Sabre board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix DDR bus width with i.MX6DL-Sabre board

Jump to solution
1,444 Views
torus1000
Contributor V

Hi,
Now I try to check i.MX6S performance with i.MX6DL-Sabre board.
I think big difference between i.MX6S and i.MX6DL are core number and DDR bus width.
I only know how to disables one of dual core.

Does anyone know how to fix DDR bus width to x32?

Is it available to set 01 to MDCTL[DSIZ] after kernel bootup?
(Running change is OK for it?)

Thanks

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,254 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

DDR bus width can be set when DDR is initialized in Uboot

flash_header.S. It can not be changed after kernel bootup.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,255 Views
igorpadykov
NXP Employee
NXP Employee

Hi torus1000

DDR bus width can be set when DDR is initialized in Uboot

flash_header.S. It can not be changed after kernel bootup.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply