How to enter USB serial download mode in software

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to enter USB serial download mode in software

跳至解决方案
14,105 次查看
patrickwood
Contributor II

We have a DualLite board that won't be easily accessible where we may need to put it into serial download mode for software upgrades.  Is there any way to do this through software?  There's a recovery button on the board, but we'd like the upgrades to be automated (also access to this button requires taking off a cover).

标签 (2)
1 解答
11,180 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Patrick,

If you are able to get into the U-boot prompt then you can do:

=> bmode usb

resetting ...

(USB download mode is entered).

You can then load u-boot.imx via USB using imx_usb_loader:

On the PC host: sudo ./imx_usb u-boot.imx

Then you will see U-boot messages on console.

Regards,

Fabio Estevam

在原帖中查看解决方案

0 项奖励
回复
10 回复数
11,180 次查看
dav1
Contributor V

Waking up this old thread. I'd like to see this functionallity on the imx8 mini's as well.

Any plans to add support in u-boot for this? 

11,181 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Patrick,

If you are able to get into the U-boot prompt then you can do:

=> bmode usb

resetting ...

(USB download mode is entered).

You can then load u-boot.imx via USB using imx_usb_loader:

On the PC host: sudo ./imx_usb u-boot.imx

Then you will see U-boot messages on console.

Regards,

Fabio Estevam

0 项奖励
回复
4,348 次查看
Vamsi080
Contributor I

Hi ,

This is vamsi Im unable to set my nxp im6 sabre sd into serial download mode.. i gave the commands bmode usb in U-Boot console. but i dont know proper dpi switches how to set there are 8 switches is there. tell me how to set . if i run bmode usb it is showing like resetting ... please help to my concern.

 

Thank You,

Vamsi.

0 项奖励
回复
11,181 次查看
joëlesponde
Contributor III

FYI, this command is broken within the mainline U-Boot if a bootable qspi flash is connected to the SOC since the version 2016.11.

The CFG1 value is now equal to 0x10 (QSPI boot) instead of 0x01:

git.denx.de Git - u-boot.git/blob - arch/arm/cpu/armv7/mx6/soc.c 

0 项奖励
回复
11,181 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Joel,

Which SoC are you using? 

Are you able to determine which commit broke bmode in your usecase?

Does 2017.05 work for you?

Thanks,

Fabio Estevam

0 项奖励
回复
11,180 次查看
joëlesponde
Contributor III

Hi,

I am using the SOC iMX6UL.

The commit that broke this feature is this one:

http://git.denx.de/?p=u-boot.git;a=commit;h=81c4eccb55ccbe4a7bb4016b23738c3c57dc364d

I reverted back to the value 0x01 and it works well.

2017.05 and 2017.07 have the same code for bmode usb.

0 项奖励
回复
11,181 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Joel,

Could you please report this problem to the U-Boot list (u-boot@lists.denx.de ) with the folks of the offending commit on Cc?

Thanks

0 项奖励
回复
11,181 次查看
patrickwood
Contributor II

Just to elaborate, I found this code in arch/arm/cpu/armv7/mx6/soc.c:

void boot_mode_apply(unsigned cfg_val)

{

    unsigned reg;

    struct src *psrc = (struct src *)SRC_BASE_ADDR;

    writel(cfg_val, &psrc->gpr9);

    reg = readl(&psrc->gpr10);

    if (cfg_val)

        reg |= 1 << 28;

    else

        reg &= ~(1 << 28);

    writel(reg, &psrc->gpr10);

}

/*

* cfg_val will be used for

* Boot_cfg4[7:0]:Boot_cfg3[7:0]:Boot_cfg2[7:0]:Boot_cfg1[7:0]

* After reset, if GPR10[28] is 1, ROM will copy GPR9[25:0]

* to SBMR1, which will determine the boot device.

*/

cfg_val is 0x01 in the case of "bmode usb".  None of these bits are documented in the RM, BTW.

0 项奖励
回复
11,181 次查看
patrickwood
Contributor II

And on android, via the "reboot download" command in the shell.

0 项奖励
回复
11,181 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Patrick

one can look at SDK file system_util.c:

/* enter the ROM Serial Download Protocol */

    hab_rvt_failsafe();

"MX6_PLATFORM_SDK "

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

Best regards

igor

0 项奖励
回复