How to enable spidev on i.MX6 using kernel 3.14.28?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable spidev on i.MX6 using kernel 3.14.28?

1,702 次查看
yaolinchang
Contributor I

Hi All,

      We run imx-test/mxc_spi_test/mxc_spi_test1.c to test spi device, but we can't find any spi device node in /dev/

We also can't find any "spidev" device name in device tree.

Our sample code of device tree as below:

Freescale default setting is connected to nor flash.

Can anyone tell me what is happen ? And how should I modify device tree?

================================

<imx6qdl.dtsi>

ecspi1: ecspi@02008000 {

                                        #address-cells = <1>;

                                        #size-cells = <0>;

                                        compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";

                                        reg = <0x02008000 0x4000>;

                                        interrupts = <0 31 IRQ_TYPE_LEVEL_HIGH>;

                                        clocks = <&clks IMX6QDL_CLK_ECSPI1>,

                                                 <&clks IMX6QDL_CLK_ECSPI1>;

                                        clock-names = "ipg", "per";

                                        status = "disabled";

};

=================================

<imx6qdl-sabresd.dtsi >

&ecspi1 {

        fsl,spi-num-chipselects = <1>;

        cs-gpios = <&gpio4 9 0>;

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_ecspi1>;

        status = "okay";

        flash: m25p80@0 {

                #address-cells = <1>;

                #size-cells = <1>;

                compatible = "st,m25p32";

                spi-max-frequency = <20000000>;

                reg = <0>;

        };

};

Thanks,

Best Regards,

Yao

标签 (3)
0 项奖励
回复
1 回复

1,071 次查看
igorpadykov
NXP Employee
NXP Employee

Hi YaoLin

could you try settings as shown below

How to enable spidev on i.MX6 using kernel 3.10.9?

VAR-SOM-MX6 Yocto Unit Testing V5 b2 - Variscite Wiki

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复