Hi All,
We run imx-test/mxc_spi_test/mxc_spi_test1.c to test spi device, but we can't find any spi device node in /dev/
We also can't find any "spidev" device name in device tree.
Our sample code of device tree as below:
Freescale default setting is connected to nor flash.
Can anyone tell me what is happen ? And how should I modify device tree?
================================
<imx6qdl.dtsi>
ecspi1: ecspi@02008000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-ecspi", "fsl,imx51-ecspi";
reg = <0x02008000 0x4000>;
interrupts = <0 31 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_ECSPI1>,
<&clks IMX6QDL_CLK_ECSPI1>;
clock-names = "ipg", "per";
status = "disabled";
};
=================================
<imx6qdl-sabresd.dtsi >
&ecspi1 {
fsl,spi-num-chipselects = <1>;
cs-gpios = <&gpio4 9 0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ecspi1>;
status = "okay";
flash: m25p80@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "st,m25p32";
spi-max-frequency = <20000000>;
reg = <0>;
};
};
Thanks,
Best Regards,
Yao