How to enable secure boot on IMX.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable secure boot on IMX.6

2,145 Views
jones_chang
Contributor II

Hi NXP pals,

I am confused about secure boot support.

1. Follow document Number: AN4581.pdf to complete for secure boot feature ???

2. For secure boot feature is necessary to do about Document Number: AN12056.pdf

In the other words encrypted boot support (including the dek_blob utility) is necessary for 

secure boot feature??

Thanks for your support

0 Kudos
Reply
2 Replies

1,933 Views
kalai
Contributor I

hi,

can i dubug imx board via usb without any debugger?

 

thanks

kalai

0 Kudos
Reply

1,954 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   The secure boot feature (signing), described in AN4581.pdf may be used separately,

without  encrypted boot support, described in  AN12056.

  

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply