How to enable i.mx6 DDR CLK and LVDS clk's SSC(Spread Sprectrum)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable i.mx6 DDR CLK and LVDS clk's SSC(Spread Sprectrum)?

3,164 次查看
弗雷德
Contributor I

EMC test result show DDR CLK 396MHz and 1080MHz is higher than limit. and 352M, 1056M and 1408M related to LVDS CLK 50MHz are also higher than limit. I want to SSC to DDR clk and LVDS clk to reduce the radiation for these frequency points.

But I can't find the related information in i.mx6 dl datasheet. Does anybody have the experience on this?

标签 (1)
0 项奖励
回复
2 回复数

2,348 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

for enabling please set spread spectrum for parent pll, refer to example on

enable the spread spectrum 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,348 次查看
弗雷德
Contributor I

Hi 

Thanks for your reply. Can I ask another question?

what is the limit for Modulation Frequency and Spectrum spread range? 5% or 10% or something like this.

0 项奖励
回复