How to enable USB debugging support for sabre-sd?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable USB debugging support for sabre-sd?

Jump to solution
3,999 Views
niharika
Contributor I

I am using iMX6 Sabre-sd board. I am able to boot up the board but I am not able to see the USB debugging option in settings.

Android version 4.2.2.

Model number: SABRESD-MX6DQ

Labels (2)
0 Kudos
Reply
1 Solution
3,535 Views
rickchu
Contributor IV

click "Build number" several times quickly, then developer options will be turn on.

00.png

View solution in original post

0 Kudos
Reply
4 Replies
3,535 Views
niharika
Contributor I

Thanks Rick Chu for your help..

0 Kudos
Reply
3,536 Views
rickchu
Contributor IV

click "Build number" several times quickly, then developer options will be turn on.

00.png

0 Kudos
Reply
3,535 Views
ZeeFrench
NXP Employee
NXP Employee

Hello,

Please check the FAQ in the document package (document tab, for latest JB: https://www.freescale.com/webapp/Download?colCode=IMX6_JB422_110_ANDROID_DOCS&location=null&fpsp=1&P...) , USB debugging is part of developper settings menu :

 

27 How do I enable developer settings on Android 4.2?

 

Google has hidden the developer settings in the latest version of Jelly Bean. The following steps explain how to retrieve developer settings:

• Go to the settings menu and scroll down to "About phone." Tap it.

• Scroll down to the bottom again until you see "Build number."

• Tap it seven (7) times. After the third tap, you'll see a playful dialog that says you're four taps away from being a

developer.

• Keep on tapping, until you've got the developer settings back.


Cheers, Philippe.

0 Kudos
Reply
3,535 Views
niharika
Contributor I

Hello Philippe,

Thanks for your reply. I am able to figured this out.

Thanks for your help.

Niharika.

0 Kudos
Reply