How to enable IPU device in Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable IPU device in Android

4,452 Views
paul_lee
Contributor II

Hi,

I have port android on freescale hardware.

My hardware supports the IPU.

How to add IPU device?

I am getting IPU device open failed error.

/dev/mxc_ipu is not available, how to add?

Paul.

Labels (4)
0 Kudos
Reply
5 Replies

3,668 Views
XianzhongLi
NXP Employee
NXP Employee

The same question answered in another thread

https://community.freescale.com/thread/306462

3,668 Views
paul_lee
Contributor II

Hi,

I have gone throught the

https://community.freescale.com/thread/306462

But still mxc_IPU is not registered.

Not available in "/dev/mxc_ipu"

What else changes required?

0 Kudos
Reply

3,668 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Paul,

     Freescale doesn't have android BSP for i.mx35, so you will have to do porting android to your platform. Now, Could you tell me some information about your project ?

(1)Linux kernel version you are using.

(2)If it is possible, Would you like to share BSP file with me ? Let me see it.

BSP file should be linux/arch/arm/mach-mx3/....., I need yours .  Send it to me : [email protected]

Probably, I can give you some advice.

Regards,

Weidong

3,668 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Paul,

     Which processor and BSP are you using ?

Regards,

Weidong

0 Kudos
Reply

3,668 Views
paul_lee
Contributor II

Hi,

Weidong

Processor is IMX35. I have port gingerbread_2.3.

Paul

0 Kudos
Reply