How to enable HDMI Input in kernel for i.mx8QMax

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable HDMI Input in kernel for i.mx8QMax

1,980 Views
santhosh2
Contributor IV

Hi,

 I want to connect the Camera to HDMI Input and test the video stream, so how to  enable HDMI Input in kernel in i.mx8QMax.

Regards

Santhosh Kumar S

0 Kudos
Reply
3 Replies

1,871 Views
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

currently this feature is not supported, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,870 Views
santhosh2
Contributor IV

NXP Bangalore Team Confirmed that this feature is supported.

Attached the page

0 Kudos
Reply

1,870 Views
igorpadykov
NXP Employee
NXP Employee

this image is general description.

Note this part is not publicly released yet and linux does not support

all its functionality.

Best regards
igor

0 Kudos
Reply