How to enable CONFIG_PCIEAER in iMX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable CONFIG_PCIEAER in iMX6Q

1,156 次查看
coreyluckhaupt
Contributor I

iMX6Q

I am using Linux Kernel 3.10.17

BSP = yocto dasiy

i am having issues with the Linux Kernel crashing, i believe this is due to a PCIe issue since i have seen the FATAL ERROR on my PCIe Switch enabled.

i am Trying to enable the Advance Error Reporting for PCIe CONFIG_PCIEAER but that option is not in the make menuconfig.

how can i enable this configuration?

标签 (3)
0 项奖励
回复
1 回复

943 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Corey

seems this is not implemented in current BSPs, one can try latest 4.x kernels

LKML: Greg KH: Linux 4.4.4

and look at efforts

Linux kernel hack for calming down a flood of PCIe AER messages

note NXP has Professional Services for customizations.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复