How to enable A7 LDO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to enable A7 LDO?

5,074 Views
stanley_yeh
Contributor II

Hi,

I am using i.MX7ULP now and I want to enable A7 LDO.

I got some clues in 36.2.3.1 of IMX7ULPRMV2_RevC.pdf.

However, I don't know how to modify the parameter (please refer to the following image) of eFuse.

As I know, once the parameter be enabled, M4 will set PMC_0_CTRL[LDOEN] bit and the current of A7 domain will be from the internal LDO. Isn't it?

In addition, I can't find "fuse map" in the document as well.

Could you help me, please?

Image 11.png

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

4,963 Views
stanley_yeh
Contributor II

Hi igorpadykov,

Thank you for your help.

In addition, if I want to set the "A7 LDO Enable" bit as 1, which value of u-boot command is correct?

A. fuse prog 2 3 0x00000001

B. fuse prog 2 3 0x01000000

Thanks a lot.

pastedImage_1.png

0 Kudos
Reply

4,963 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stanley

 for fuses programming one can look on

Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog 

Best regards
igor

0 Kudos
Reply

4,963 Views
stanley_yeh
Contributor II

Hi igorpadykov,

I know how to program.

What I don't know is the address order, little-endian or big-endian?

In the Bank 2 Word 3, the byte order is "0x530 0x531 0x532 0x533" or "0x533 0x532 0x531 0x530"?

If I want to set the "A7 LDO Enable" bit as 1, which value of u-boot command is correct? 0x00000001 or 0x01000000?

Thanks.

0 Kudos
Reply

4,962 Views
igorpadykov
NXP Employee
NXP Employee

Hi Stanley

fuse map can be found in attachment section of Reference Manual,

also attached below.

i.MX 7ULP Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply