How to do for nand boot config"boot search count"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to do for nand boot config"boot search count"?

Jump to solution
1,972 Views
翔李
Contributor IV

HI,

I plan to design a car board on imx6 solo,to boot from SD3 or 256MB nand flash,When insert a TF card it selects SD3 boot,else boot from nand.

BOOT_CFG2[4:3]=10 to select SD3,so,wneh to select nand boot,the BOOT_CFG2[4:3] select which one?The nand IC is winbond W29N02GVSIAA.

What is meaning of"boot search count"?

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

0 Kudos
Reply
1 Solution
1,698 Views
翔李
Contributor IV
0 Kudos
Reply
4 Replies
1,698 Views
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to sect. 8.5.2.3 Firmware Configuration Block i.MX6DQ Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf 


The FCB is the first sector in the first good block. The FCB should be present at each
search stride of the search area.
The search area contains copies of the FCB at each stride distance, so in case the first
NAND block becomes corrupted, the ROM will find its copy in the next NAND block.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,698 Views
翔李
Contributor IV

HI,

Thanks.

But,I do not know which number for me to select,00?01?10?11?I am poor in NAND boot,sorry.

In my board,can I select 10-4 for boot search count nand falsh?

pastedImage_1.png

0 Kudos
Reply
1,698 Views
igorpadykov
NXP Employee
NXP Employee

please check settings for i.MX6 Sabre AI board which uses NAND

Schematics (5)
Design files for i.MX 6Quad and i.MX 6DualLite CPU1 Cards
Design files for Base Board (REV E)

http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Linux Guide in Linux Documentation

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor

1,699 Views
翔李
Contributor IV

THANKS.

0 Kudos
Reply