How to display monitor via USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to display monitor via USB

1,875件の閲覧回数
wangvictor
Contributor III

Hi All,

I'm using i.MX6 sabresd  DL for my cpu and linux kernel driver for version 4.1.15.

I'm trying to display the monitor via USB.

Which driver I should open and build in?

And what else I have to do ?

Thanks in Advance!

ラベル(5)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,702件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi victor

seems one needs to implement support for usb monitor driver described on

http://www.usb.org/developers/docs/devclass_docs/usbmon10.pdf 

Chapter 39 CHIPIDEA USB Driver attached Linux Manual describes

current lnux usb driver capabilities.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,702件の閲覧回数
wangvictor
Contributor III

Is this just can support X86 structure CPU ?

Or I can using on the ARM structure?

0 件の賞賛
返信