I would like to disable the gstreamer in NXP-BPS for iMX8M Mini EVK for some test reasons. How can I do This?
I removed "packagegroup-fsl-gstreamer1.0-full" and "packagegroup-fsl-gstreamer1.0" from the CORE_IMAGE_EXTRA_INSTALL list, but it still tries to build the gstreamer.
Thank you in advance and best regards
Elmar Albert
Could you tell us which version BSP are you using? You can refer to the thread https://community.nxp.com/message/1071170 , I am working on it for you , when I get the method I will tell you as soon as possible.
Hello Rita,
thank you for your response. I'm using sumo-4.14.98-2.0.0_ga.
The main reason, why I wanted to disable the gstreamer was regarding some build issus, which are solved now.
But anyway I'm interested in how to disable it.
Thank you and regards
Elmar
Hi Elmar Albert,
You can also try by adding below line in local.conf:
BAD_RECOMMENDATIONS = "gstreamer gstreamer1.0"
It will not install gstreamer, however it will also give you indication in form of error regarding which other packages needs gstreamer.
Regards,
Karan Gajjar