In the latest Yocto BSP (4.14.98_ga / sumo) I added a custom machine for our i.MX8M mini machine, added some kernel patches, and some U-Boot patches. All this works fine for i.MX8M Mini. Now I am trying to do this for our i.MX6 based CoMs. It fails when building U-Boot. We don't need U-Boot, because for i.MX6 CoMs we have our own U-Boot. Is there a way when building core-image-minimal to configure "dont build u-boot" ?
Thanks in advance
解決済! 解決策の投稿を見る。
 
					
				
		
For now I figured out, how to skip it in current Yocto Sumo release.
Use the following command to skip dependencies u-boot and u-boot-imx in building core-image-minimal.
It is important to say, that IMAGE_FSTYPES_remove = has to contain "sdcard". Sdcard image needs u-boot to work.
bitbake -I u-boot -I u-boot-imx  core-image-minimalYou can also set this as a variable:
https://www.yoctoproject.org/docs/current/bitbake-user-manual/bitbake-user-manual.html
Let me know if there is any better solution.
Regards
Markus
 
					
				
		
For now I figured out, how to skip it in current Yocto Sumo release.
Use the following command to skip dependencies u-boot and u-boot-imx in building core-image-minimal.
It is important to say, that IMAGE_FSTYPES_remove = has to contain "sdcard". Sdcard image needs u-boot to work.
bitbake -I u-boot -I u-boot-imx  core-image-minimalYou can also set this as a variable:
https://www.yoctoproject.org/docs/current/bitbake-user-manual/bitbake-user-manual.html
Let me know if there is any better solution.
Regards
Markus
 
					
				
		
 gusarambula
		
			gusarambula
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hello Markus Bauer,
Thank you for sharing your findings! I'm sure they will help other community users.
Theoretically you could also use IMAGE_INSTALL_remove += "u-boot-imx" provided that you take into consideration dependencies like removing the sdcard FSTYPE as you pointed out.
Regards,
 
					
				
		
Hello,
from my understanding, recipes providing bootloader - may it be uboot-imx our your private U-Boot clone or whateverer - should add in their recipe:
PROVIDES = "virtual/bootloader"
That way, you are able
- to depend on virtual/bootloader in generic recipes
- to add PREFERRED_PROVIDER_virtual/bootloader = "your bootloader recipe" to select the bootloader in your machine.conf file
Besides that, if you do not need a bootable image, you can of course remove from IMAGE_FSTYPES
Regards,
Markus
 
					
				
		
Hi Markus Bauer,
One can refer the below link to disable building of U-boot.
https://community.nxp.com/thread/318106
Regards,
Radhika Somaiya.
 
					
				
		
Hey radhika.somaiya@volansystech.com
I've already tried the solutions mentioned there. I don't know what to do with the lines of the files mentioned in the post you linked. Also this post is from 2014, maybe things have changed?
Setting `IMAGE_BOOTLOADER = ""` results in an error also.
Regards
Markus