How to disable USB3.0 and force USB3.0 to USB2.0 in kernel config for maaxboard and maaxboard-mini?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to disable USB3.0 and force USB3.0 to USB2.0 in kernel config for maaxboard and maaxboard-mini?

Jump to solution
2,300 Views
gonewithwind-peter
Senior Contributor I

hi all

I use maaxboard and maaxboard-mini board, we need to connect a USB disk(2.0 and 3.0),

but after insert USB3.0 disk, there is an error  ,  someone posted before here and need to update the kernel :https://community.nxp.com/t5/i-MX-Processors/USB3-0-disconnect-periodic-on-i-mx8mq/m-p/1155828/highl...

I do not want change to new yocto branch(too much work,  our node code not work...).

can I and how to disable USB3.0 and force USB3.0 to USB2.0 in kernel config?

 

Thank you very much.

0 Kudos
Reply
1 Solution
2,292 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

unfortunately there is no software way to disable USB3.0.

i.MX8M Mini has not USB3.0.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
2,287 Views
gonewithwind-peter
Senior Contributor I

@igorpadykov 

thanks. got it

0 Kudos
Reply
2,293 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

 

unfortunately there is no software way to disable USB3.0.

i.MX8M Mini has not USB3.0.

 

Best regards
igor

0 Kudos
Reply