Dear Community,
To rule out the impact of MCLK frequency to other high speed interfaces on our custom PCB based on iMX8MP, we have a need to enable/disable the MIPI-CSI2 camera driver in order to enable /disable the MCLK clock:
I re-built the ov5640_mipi_v2.c as loadable kernel module :
diff --git a/arch/arm64/configs/imx_v8_defconfig b/arch/arm64/configs/imx_v8_defconfig
index a8a46508482d..a096230294d3 100644
--- a/arch/arm64/configs/imx_v8_defconfig
+++ b/arch/arm64/configs/imx_v8_defconfig
@@ -528,7 +528,7 @@ CONFIG_VIDEO_MXC_CAPTURE=y
CONFIG_VIDEO_MX8_CAPTURE=y
CONFIG_VIDEO_MXC_CSI_CAMERA=y
CONFIG_MXC_MIPI_CSI=y
-CONFIG_MXC_CAMERA_OV5640_MIPI_V2=y
+CONFIG_MXC_CAMERA_OV5640_MIPI_V2=m
CONFIG_V4L_MEM2MEM_DRIVERS=y
CONFIG_SDR_PLATFORM_DRIVERS=y
CONFIG_VIDEO_IMX219=m
I saw the in remove() function, clk_disable_unprepare(sensor->sensor_clk) is called. But the 24-MHz MCLK still persists after rmmod.
static int ov5640_remove(struct i2c_client *client)
{
struct v4l2_subdev *sd = i2c_get_clientdata(client);
struct ov5640 *sensor = to_ov5640(client);
v4l2_async_unregister_subdev(sd);
clk_disable_unprepare(sensor->sensor_clk);
ov5640_power_down(sensor, 1);
ov5640_regualtor_disable();
return 0;
}
I would like to know how to disable it completely during the removing of the module, please?
Thanks in advance and best regards,
Khang