Hi,
We compiled the Android image for SabreSD-6dq and ran our solo board but encountered a lot of FSLProfile error on runtime. I tried to remove the package installation from im6.mk but it just stuck on boot animation. Is there a easy way to debug or disable the service? Thanks.
Hi,
Did any one manage to disable the FSLProfileApp/Service?
I tried to do (like what williamtung did, removed the package installation from imx6x.mk) and android hang at animation screen.
I really want to disable this feature as it make too many confusion to the end user. For eg, the power saving mode may give you the shortest battery life and the performance mode may give you longer batter life sometimes. At other time, it may give diff result. So, I just want to simplify (just leave all core enable)
Thanks in advance.
Regards,
PK
Hi,
After Applying Those patches, Still FSLPowerService force closed error is coming on our board !!!!, we are using IMX6 solo, Android ICS 4.0.3 .
No, I'm not sure which service or node the FSLProfileAPP/Service is looking for.
I don´t have this source code installed on my machine.
Could you, please, let me know which Android.mk did you changed?
Hi Daiane,
I only change device/fsl-proprietary/pcie-wifi/Android.mk to support Intel PCIe WIFI and device/fsl/imx6/imx6.mk to add some firmware.
Ok, so It made me think that your goal is not disable FSLProfile. You´re trying to do something else, and faced those errors as a side effect.
Could you, please, share your goal?
Could you, please, share your dmesg and logcat?
Hi Daiane,
To goal is to enable FSLProfile without popping up error message. I just notice that the default profile looking for more than one core. Can you please advise which file to modify to limit to just one core?
logcat:
W/System.err( 2618): java.io.FileNotFoundException: /sys/devices/system/cpu/cpu1/online: open failed: ENOENT (No such file or director
y)
threadid=1: thread exiting with uncaught exception (group=0x40a661f8)
E/AndroidRuntime( 2618): FATAL EXCEPTION: main
E/AndroidRuntime( 2618): java.lang.RuntimeException: Unable to start service fsl.power.service.FSLPowerOptionService@410cbd58 with Intent { cmp=fsl.power.service/.FSLPowerOptionService }: java.lang.NullPointerException
E/AndroidRuntime( 2618): at android.app.ActivityThread.handleServiceArgs(ActivityThread.java:2376)
E/AndroidRuntime( 2618): at android.app.ActivityThread.access$1900(ActivityThread.java:123)
E/AndroidRuntime( 2618): at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1210)
E/AndroidRuntime( 2618): at android.os.Handler.dispatchMessage(Handler.java:99)
E/AndroidRuntime( 2618): at android.os.Looper.loop(Looper.java:137)
E/AndroidRuntime( 2618): at android.app.ActivityThread.main(ActivityThread.java:4424)
E/AndroidRuntime( 2618): at java.lang.reflect.Method.invokeNative(Native Method)
E/AndroidRuntime( 2618): at java.lang.reflect.Method.invoke(Method.java:511)
E/AndroidRuntime( 2618): at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:784)
E/AndroidRuntime( 2618): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:551)
E/AndroidRuntime( 2618): at dalvik.system.NativeStart.main(Native Method)
E/AndroidRuntime( 2618): Caused by: java.lang.NullPointerException
E/AndroidRuntime( 2618): at
fsl.power.service.FSLPowerOptionService.offlineCPU(FSLPowerOptionService.java:414)
E/AndroidRuntime( 2618): at fsl.power.service.FSLPowerOptionService.setcpuNM(FSLPowerOptionService.java:795)
E/AndroidRuntime( 2618): at fsl.power.service.FSLPowerOptionService.activeProfile(FSLPowerOptionService.java:778)
E/AndroidRuntime( 2618): at fsl.power.service.FSLPowerOptionService.onStart(FSLPowerOptionService.java:220)
E/AndroidRuntime( 2618): at android.app.Service.onStartCommand(Service.java:438)
E/AndroidRuntime( 2618): at android.app.ActivityThread.handleServiceArgs(ActivityThread.java:2359)
Hi Daiane,
I got a little time to trace the FSLProfileService code and found there are only "soc_type.MX6Q=63" and "soc_type.MX6DL=61" are defined. Since MX6SOLO shares the same ID (Major=6100), there's no way to tell it's DualLite or Solo. I can quick patch the code for my solo board but wonder if Freescale has any plan to fix this issue. Thanks.
I´m glad to hear that. I´m not used with imx6s so I was not aware of this android behavior. I had asked internally for some help for your issue. I´m glad to know you was able to fix it.
In my point of view, it´s not a bug, you´ve been using a BSP that was released to be used on another chip.
But I agree with you that it could be more "configurable".
Thanks a lot for letting us know.
Hi Daiane,
I am also facing the similar problem of "Fsl Power services stopped" and unable to solve it...
we have designed our own custom board using i.Mx6S solo processor and using Android 13.4.1 BSP... After the complete loading of the Android, the "FSL Power serives stopped" message comes on the screen and the android console " root@android:/ #" .. we are also getting a number of Android process related error, but i am unable to analyze. Pl. find attached here the screenshots of the same and Logcat for reference...
request help and guidance,
thanks in advance,
Ujala,
William is saying that you will need to modify the FSLPowerOptionService class to define separate system on chip (soc) types for the dual lite and solo (look for soc_type and differentiate between MX6DL and MX6SOLO) and then in the initPowerProfile method you will need to define a profile for the solo type that specifies how to handle the performance, power saving, and normal modes of operation (the key here is to make sure Profiles.CPUNM is assigned 0 as the source of your errors in logcat is the FSLProfileApp trying to access cores that don't exist).
Michael
Hi Michael,
Thank you very much for the accurate guidance and pin-point patch instructions.
Appologies for my little knowledge. I am really a beginner in Android and Java. Request you to pl. let me know how and where to locate the FslPowerOptionService class file in myandroid. ..? :smileysilly::smileysilly:
i understand , inside this class file , i shal be getting initPowerProfile where i shall be modifying the Profiles.CPUNUM.
Also, in the same logfile, can you let me know, how can i disable the "gps services" as on my board, i am not using any GPS, the hardware and driver is disabled in the kernel but the services are still registered and remain on . Due to that my "root@android:# " prompt is in "Hang mode" and i am unable to use it.
heartiest thanks and appreciation again for the help..
Ujala
Ujala,
Look in myandroid/packages/apps/fsl_imx_demo/FSLProfileService/src/fsl/power/service for the FSLPowerOptionService class.
As for gps, I changed the following (they're may be other items I'm missing). In init.rc, you need to remove:
symlink /dev/ttymxc1 /dev/gpsdevice
in ueventd.freescale.rc I removed:
| /dev/ttymxc2 | 0660 system | gps |
| /dev/ttya0 | 0660 system | gps |
| /dev/ptya0 | 0660 system | gps |
| /dev/ttya1 | 0660 system | gps |
| /dev/ptya1 | 0660 system | gps |
in BoardConfigArm2.mk I modified the following entries:
BOARD_HAVE_HARDWARE_GPS := false
USE_ATHR_GPS_HARDWARE := false
The following entry should already be false:
USE_QEMU_GPS_HARDWARE := false
Michael
Hi Michael,
Thanks a lot from the bottom of my heart. Your support
is heartily appreciated...
I am able to patch the file as guided by
you and solve the " Fsl Power profile stopped" problem.
Besides,
thanks you so much for the stepwise guidance on GPS disable procedure.
Although, with my own knowledge, some searching and surfing in community
and some understanding, i was able to disable GPS services yesterday by
myself by going into init,freescale.rc. However i was not sure of my
random steps and its repercussions , if any. Your stepwise procedure ,
in that way was able to reassure me of of my own understanding and was
really relieving.
Thanks again for all your support and help.
could
you pl. help help me with some steps in finding out the display screen
related resolution, size or configuration settings and CTP idc
registration procedure. I am facing below related issues:
1. The
virtual key pad of android is not behaving correctly and when i touch
the keys, the correct keys are not coming on screen else other keys are
appearing. pl. see the attached snap. when i touch "P" on the keypad
actually "i" is appearing and when i touch "O" then "u is appearing...
All the keys appear to be shifted both horizontally and vertically.. its
really peculiar and i am not finding any clue on that.
2. Even though
my touch panel is registered but the logcat messages are below
below:
a.
W/imx6.gralloc( 2155): xres = 800 px
W/imx6.gralloc( 2155):
yres = 480 px
W/imx6.gralloc( 2155): xres_virtual = 800
px
W/imx6.gralloc( 2155): yres_virtual = 1536 px
b.
" Touch device
'cast-touch' could not query the properties of its associated display 0.
The device will be inoperable until the display size becomes available.
"
I am simply clueless on the above except this understanding that
these must be some Android related settings in some config files..
request your help and guidance , if possible..
thanks again for your
openness and all the help,
---
Warm regards,
Ujala Kumar
On
09-05-2013, Michael Robbeloth wrote:
HOW TO DISABLE
FSLPROFILEAPP/SERVICE
created by Michael Robbeloth 1 in _i.MX
Community_ - View the full discussion 2
Ujala,
I'm not sure what the issue could be with your touchscreen. We use a two-touch capacitive touchscreen so the registration process is not necessary on our device. I would try reposting as a new forum message and see if anyone can offer their assistance.
Michael
Hi Jimmy,
Our board is based on the SabreLite and I'm using Android 13.4.1 BSP.
William,
This is something my company is looking to do on a solo board as well. If anyone has any good approaches, please let us know. Thanks.
Michael