How to debug using JTAG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to debug using JTAG

2,810 Views
BryanJI
Contributor I

How to setup an environment which I can use JTAG to debug the program?

Because when you first get a new design, you need to figure out the problem of your DDR2.

If you can't setup DDR2, nothing you can to to boot from SD, am I right?

 

Any solutions.

Labels (1)
0 Kudos
Reply
3 Replies

2,602 Views
RichardXiao
Fresh Out Contributor
0 Kudos
Reply

2,601 Views
BryanJI
Contributor I
Before I use Linux BSP, I need to make sure my custom board running correctly. It is better I can use IRA or similar IDE with J-Link to figure out the reason. Possibly, DDR configuration error. It helps me to find the reason quickly and efficient. 


Robert M Girard said:

Hello Bryan,

Are you using the Linux BSP for the i.MX28 EVK?

 

Regards

Robert G

0 Kudos
Reply

2,602 Views
RobertMGirard
Contributor I

Hello Bryan,

Are you using the Linux BSP for the i.MX28 EVK?

 

Regards

Robert G

0 Kudos
Reply