How to debug the LEC-IMX8MP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to debug the LEC-IMX8MP

2,779件の閲覧回数
SegFault0
Contributor II

Hello,

what are the options for debugging the Cortex-M7 on my LEC-IMX8MP modul. The datasheet from Adlink states that there should be a 30-pin Header with 5 pins for the JTAG interface. Unfortunately, that interface is missing on my modul. Are there any other options, like debugging from the Cortex-A or at least debug traces? 

 

Edit: Adlink support supplied me with the pinout

0 件の賞賛
返信
3 返答(返信)

2,768件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean your board doesn't have any debug interface?

0 件の賞賛
返信

2,763件の閲覧回数
SegFault0
Contributor II

It technically does, but the 30-Pin header, of which 5 pins are reserved for JTAG are missing. I could solder them on myself, but Adlink does not supply a pinout or any schematics for the board, so I'm kind of lost.

On page 13 they state that there should be a connector, which is simply missing on my board. 

LEC-IMX8Mplus User guide (adlinktech.com)

タグ(1)
0 件の賞賛
返信

2,749件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

maybe you can refer to the chapter 9 Linux Remote Processor (RPROC) framework

"https://www.nxp.com.cn/docs/en/application-note/AN5317.pdf"

0 件の賞賛
返信