How to create u boot spl and ubl for imx7d

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create u boot spl and ubl for imx7d

2,657件の閲覧回数
atakanakbulut
Contributor II

Hello i need u boot spl and ubl for imx7 i find this topic but not prepared for imx7 and other processors

i need this extensions 

u-boot-spl.ubl

u-boot.ubl

u-boot-spl.bin

how to creat u-boot-spl.bin in u-boot2014.04? 

FabioEstevam

0 件の賞賛
返信
3 返答(返信)

2,353件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You can build the cl-som-imx7_defconfig target, which is a mx7 board with SPL support.

The resultant binaries are SPL and u-boot.img and they can be flashed directly into the SD card/eMMC.

Regards,

Fabio Estevam

0 件の賞賛
返信

2,353件の閲覧回数
atakanakbulut
Contributor II

Thank you your comment , i am using u-boot.imx for sd card but i need write to nand this image , our old card prepared for spl and u-boot.img Can i prepare for u-boot.imx ? Hardware , mtd nand is ready and i did not want use to mfgtools actually i hate this and not export usb port our custom card . Which way i should try ? i did not any example mtd0 mtd1 nand and u-boot.imx 

thank you

0 件の賞賛
返信

2,353件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

In order to flash the NAND you need to use a tool called imx-kobs.

0 件の賞賛
返信