How to create a hci interface in imx7 Sabre Board ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to create a hci interface in imx7 Sabre Board ?

1,000 次查看
ganeshrajask
Contributor I

Hello everyone,

I am working on imx7 sabre board. I have built Yocto package BSP (krogoth with kernel version 4.1.15) and flashed it to the board. I have checked Wi-FI interface via GUI. Now I want to test Bluetooth. How do I test bluetooth ? Which firmware to use when using hciattach tool ? What other parameters to pass to hciattach tool to create hci interface ?

Thanks in advance.

Ganesh Raja S K

标记 (1)
0 项奖励
回复
1 回复

880 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ganesh

please download Broadcom firmware package

BCMDHD-L4.1.15_2.0.0
https://www.nxp.com/webapp/Download?colCode=BCMDHD-L4.1.15_2.0.0&appType=license&Parent_nodeId=13376...

also vendor provides additional Quick Start documents, please ask them on

 wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-nxp-i-mx.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复