How to convert Schematics to xml file IOMUX TOOL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to convert Schematics to xml file IOMUX TOOL?

1,205 Views
prasannaprabhu7
Contributor III

Hi All,

I am working for a project on WEC7 for a customer for board bring up on IMX6  Solo processor. Was going through this IMX tool in forum and was thinking to use the same for first time, where I have schematics given by  customer and freescale IOMux tool. Can anyone help me generating xml file out of .pdf schematics to try out IOMux tool to generate MUX configuration ?

Thanks in advance,

Regards,

Prasanna Prabhu

Labels (6)
0 Kudos
Reply
1 Reply

971 Views
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid we do not have tool – to generate IOMUX configuration using

schematic file (although it is good idea). Mainly this should be implemented

manually.  

  Note, when configuring GPIO, the Processor Expert for i.MX  may be useful.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX

https://community.freescale.com/docs/DOC-101470 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply