How to convert Schematics to xml file IOMUX TOOL?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to convert Schematics to xml file IOMUX TOOL?

1,167件の閲覧回数
prasannaprabhu7
Contributor III

Hi All,

I am working for a project on WEC7 for a customer for board bring up on IMX6  Solo processor. Was going through this IMX tool in forum and was thinking to use the same for first time, where I have schematics given by  customer and freescale IOMux tool. Can anyone help me generating xml file out of .pdf schematics to try out IOMux tool to generate MUX configuration ?

Thanks in advance,

Regards,

Prasanna Prabhu

ラベル(6)
0 件の賞賛
返信
1 返信

933件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   I am afraid we do not have tool – to generate IOMUX configuration using

schematic file (although it is good idea). Mainly this should be implemented

manually.  

  Note, when configuring GPIO, the Processor Expert for i.MX  may be useful.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PROCESSOR-EXPERT-IMX

https://community.freescale.com/docs/DOC-101470 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信