How to connect a NAND Flash with the i.MX6 microprocessor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect a NAND Flash with the i.MX6 microprocessor

1,180 次查看
carlosreverbel
Contributor I

Hello,

   I am working on a project to build a custom board for the i.MX6D microprocessor and I would like to use mfgtool to save the bootloader and the O.S. in a NAND Flash chip. The problem is that I cannot find which pins of the microprocessor to connect to the NAND Flash. Could you provide me an schematic showing how to connect the chip to the i.MX6D microprocessor? 

Thank you.

标记 (2)
0 项奖励
回复
1 回复

999 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the SABRE for Automotive Infotainment:

https://www.nxp.com/webapp/Download?colCode=SABRE-AI-QUAD-CPU2&Parent_nodeId=1413216565594727840052&... 

https://www.nxp.com/webapp/Download?colCode=SABRE-AI-DUALLITE-CPU2&Parent_nodeId=1413216565594727840... 

SABRE-2|Automotive-Infotainment|i.MX6|NXP 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复