How to connect EIM for i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect EIM for i.MX6SL

1,459 次查看
ko-hey
Senior Contributor II

Hi all

Let me confirm about the connection of EIM for i.MX6SL.

My customer plan to boot from NOR-SPI flash(16bit).

pastedImage_1.png

In that case, is the above connection correct ?

P.S.

I refer to the following link.

https://community.nxp.com/message/437106

Ko-hey

标签 (1)
0 项奖励
回复
3 回复数

1,309 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

it is correct with left column should be AUS=0 Address shifted according to port size,

connecting the address signals one to one (for example, A0→A0 and A1→A1).

and right column should be AUS=1.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,309 次查看
ko-hey
Senior Contributor II

Hi

Is following table correct ?

AUS=0

AUS=1

NOR

ADDRESS

EIM_ADDR[22]

EIM_ADDR[23]

A[22]

EIM_ADDR[21]

EIM_ADDR[22]

A[21]

EIM_ADDR[20]

EIM_ADDR[21]

A[20]

EIM_ADDR[19]

EIM_ADDR[20]

A[19]

EIM_ADDR[18]

EIM_ADDR[19]

A[18]

EIM_ADDR[17]

EIM_ADDR[18]

A[17]

EIM_ADDR[16]

EIM_ADDR[17]

A[16]

EIM_AD[15]

EIM_ADDR[16]

A[15]

EIM_AD[14]

EIM_AD[15]

A[14]

EIM_AD[13]

EIM_AD[14]

A[13]

EIM_AD[12]

EIM_AD[13]

A[12]

EIM_AD[11]

EIM_AD[12]

A[11]

EIM_AD[10]

EIM_AD[11]

A[10]

EIM_AD[9]

EIM_AD[10]

A[9]

EIM_AD[8]

EIM_AD[9]

A[8]

EIM_AD[7]

EIM_AD[8]

A[7]

EIM_AD[6]

EIM_AD[7]

A[6]

EIM_AD[5]

EIM_AD[6]

A[5]

EIM_AD[4]

EIM_AD[5]

A[4]

EIM_AD[3]

EIM_AD[4]

A[3]

EIM_AD[2]

EIM_AD[3]

A[2]

EIM_AD[1]

EIM_AD[2]

A[1]

EIM_AD[0]

EIM_AD[1]

A[0]

DATA

LCD_DAT[21]

LCD_DAT[21]

DQ[15]

LCD_DAT[20]

LCD_DAT[20]

DQ[14]

LCD_DAT[19]

LCD_DAT[19]

DQ[13]

LCD_DAT[18]

LCD_DAT[18]

DQ[12]

LCD_DAT[17]

LCD_DAT[17]

DQ[11]

LCD_DAT[16]

LCD_DAT[16]

DQ[10]

LCD_DAT[15]

LCD_DAT[15]

DQ[9]

LCD_DAT[14]

LCD_DAT[14]

DQ[8]

LCD_DAT[13]

LCD_DAT[13]

DQ[7]

LCD_DAT[12]

LCD_DAT[12]

DQ[6]

LCD_DAT[11]

LCD_DAT[11]

DQ[5]

LCD_DAT[10]

LCD_DAT[10]

DQ[4]

LCD_DAT[9]

LCD_DAT[9]

DQ[3]

LCD_DAT[8]

LCD_DAT[8]

DQ[2]

LCD_DAT[7]

LCD_DAT[7]

DQ[1]

LCD_DAT[6]

LCD_DAT[6]

DQ[0]

Ko-hey

0 项奖励
回复

1,309 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

 

yes correct

 

Best regards
igor

0 项奖励
回复