How to configure DDR initialization script with 933MHz DDR3LMemory ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to configure DDR initialization script with 933MHz DDR3LMemory ?

1,777 次查看
peteramond
Contributor V

Hi All,

This is a custom hardware design with;

Processor - iMAX6Q - MCIMX6Q6AVT10AC

RAM - 933MHz Micron DDR3L - MT41K256M16TW-107 IT:P

1) Here is the configuration for the script. Can you check and tell me the configurations are correct or not ?

pastedImage_2.png

2) Don't you have different script generator for DDR3L type memories (Low Power RAM) ? 

3) In memory type I don't have to select DDR3L-933 option. What should I select ?

4) In DRAM clock frequency I don't have to select any option for 933MHz. What should I select ?

5) Under SI configuration section what should I select for 

DRAM DSE Setting - DQ/DQM (ohm)

DRAM DSE Setting - ADDR/CMD/CTL (ohm)

....etc.

Can you give me an idea on this SI configuration parameters. Under which conditions of the memory should we change those values and how ?

Waiting for a detailed explanation for this. 

Regards & Thanks,

Peter.

标签 (4)
0 项奖励
回复
1 回复

1,292 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Customers can use DDR3 script for i.MX6Q:

i.MX6DQ SABRE SDP/B DDR3 Register Programming Aid 

Also, the following may be helpful:

Freescale i.MX6 DRAM Port Application Guide-DDR3 

I.MX6 MMDC supports memory up to 532MHz, there fore all timings

should be selected based on this maximal frequency, say DDR3-800 or DDR3-1060


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复