How to configure ADV7182 decoder with IMX6ull processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure ADV7182 decoder with IMX6ull processor?

9,703件の閲覧回数
riguangpeng
Contributor I

Hello everyone,

I have a custom board that has an IMX6ull processor and it is connected to a video decoder ADV7182. The version of linux kernel is 4.1.15. I want to configure it to capture video from an analogue camera.  

Can you help me how to configure the kernel or how to patch the linux kernel?

ラベル(2)
0 件の賞賛
返信
9 返答(返信)

9,488件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi riguang peng,

   Our i.MX6QDL Sabreauto EVK supports ADV7180, you can refer to it for your design.

arch/arm/boot/dts/imx6qdl-sabreauto.dtsi

 

... ...

        i2c@1 {
            #address-cells = <1>;
            #size-cells = <0>;
            reg = <1>;

            adv7180: adv7180@21 {
                compatible = "adv,adv7180";
                reg = <0x21>;
                pinctrl-names = "default";
                pinctrl-0 = <&pinctrl_ipu1_1>;
                clocks = <&clks IMX6QDL_CLK_CKO>;
                clock-names = "csi_mclk";
                DOVDD-supply = <&reg_3p3v>; /* 3.3v, enabled via 2.8 VGEN6 */
                AVDD-supply = <&reg_3p3v>;  /* 1.8v */
                DVDD-supply = <&reg_3p3v>;  /* 1.8v */
                PVDD-supply = <&reg_3p3v>;  /* 1.8v */
                pwn-gpios = <&max7310_b 2 0>;
                csi_id = <0>;
                mclk = <24000000>;
                mclk_source = <0>;
                cvbs = <1>;
            };

... ...

 

adv7180 driver:

linux_top/drivers/media/platform/mxc/capture/adv7180.c

Have a nice day!

BR,

Weidong

0 件の賞賛
返信

9,488件の閲覧回数
riguangpeng
Contributor I

Hi Wigros Sun, Thank you

Now, I config my dts as flowing:

&i2c2 {
        clock_frequency = <100000>;
        pinctrl-names = "default";
          pinctrl-0 = <&pinctrl_i2c2>;
          status = "okay";

            adv7182: adv7182@20 {
                     compatible = "adv,adv7180";
                     reg = <0x20>;
                     pinctrl-names = "default";
                     pinctrl-0 = <&pinctrl_csi1>;
                    clocks = <&clks IMX6UL_CLK_CSI>;
                     clock-names = "csi_mclk";
                    //pwn-gpios = <&gpio_spi 6 1>;
                     //rst-gpios = <&gpio_spi 5 0>;
                     csi_id = <0>;
                    //mclk = <24000000>;
                    //mclk_source = <0>;
                    mclk = <28636300>;
                     mclk_source = <0>;
                     status = "okay";


                      port {
                                  adv7182_ep: endpoint {
                                   remote-endpoint = <&csi1_ep>;
                                 };
                          };
             };
};

&csi {
         status = "okay";
         //pinctrl-names = "default";
         //pinctrl-0 = <&pinctrl_csi1>;


         port {
                       csi1_ep: endpoint {
                       remote-endpoint = <&adv7182_ep>;
                       };
               };
};

then I patch the mx6s_capture.c  according to 0001-Enable-CSI-support-BT656-interlace-and-add-adv7180.patch.zip, I do not change the drivers/media/platform/mxc/capture/adv7180.c.

Do you have any other advice?

0 件の賞賛
返信

9,488件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

   你的硬件连接方式,要和dts里的节点对应上。

                    pwn-gpios
                    rst-gpios

这2个是电源控制和reset控制,你的电路上没有吗?

ADV7180的驱动里会读取和处理dts节点里的配置,然后再处理。你要根据你的硬件配置节点,而且要微调一下adv7180.c

weidong

0 件の賞賛
返信

9,489件の閲覧回数
riguangpeng
Contributor I

硬件设计上是有的,我配置上!还有就是时钟频率是24M吧。

0 件の賞賛
返信

9,487件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

这是Sabre AI板子上的ADV7180电路,和你的对比一下配置,它的dts怎么配置,你的就怎么配置。 第12页。

0 件の賞賛
返信

9,487件の閲覧回数
riguangpeng
Contributor I

现在我的视频流能够出来了,但是颜色不对,感觉是ADV7182A寄存器配置的问题,请指导怎样配置捕获.PNG

0 件の賞賛
返信

9,487件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

关于ADV7182A寄存器配置的问题,你最好能够请求ADI的FAE或者他们代理的FAE来帮你配置,因为不是我们的芯片,我们也没有原厂熟悉。

另外使用模拟摄像机,你需要注意

(1)制式一致性

摄像头制式(PAL,NTSC), ADV7182A制式配置,mxc_v4l2_capture.c(这是CPU端捕获驱动)中制式跟踪一下,三者是否是一致的;

(2)YUV输出协议

一般我们都会用BT.656格式输出,那么VSYN/ HSYNC都会编码在data的8bit数据线上,你不需要外部连接HSYNC/VSYNC信号。

(3)camera的上电

我们要求camera先上电,对你的系统来说,就是camera和ADV7182A先上电。

你先按照上面的建议检查一下,然后再请去寻求相关支持。

Have a nice day!

BR,

Weidong

0 件の賞賛
返信

9,486件の閲覧回数
riguangpeng
Contributor I

技术支持:你好!

已经初步这个问题,是由于RGB三个颜色都缺色的问题,data0-data7上都有数据信号,具体是哪里的问题,还在分析中,另外还有一个问题,就是视频的延迟比较大,在1S秒左右,这个延迟优化有什么建议吗?

0 件の賞賛
返信

9,486件の閲覧回数
riguangpeng
Contributor I

好的,谢谢哦。

0 件の賞賛
返信