How to compile the gstreamer code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to compile the gstreamer code

7,154件の閲覧回数
santhosh2
Contributor IV

I am trying to write a gstreamer code and compile for i.mx8Qmax. But when i try to compile im facing a problem

santhosh@santhosh-Vostro-15-3568:~/Desktop/gstreamer$ echo $CC
aarch64-poky-linux-gcc --sysroot=/opt/fsl-imx-x11/4.9.51-mx8-beta/sysroots/aarch64-poky-linux
santhosh@santhosh-Vostro-15-3568:~/Desktop/gstreamer$ aarch64-poky-linux-gcc basic-tutorial-1.c -o basic-tutorial-1 `pkg-config --cflags --libs gstreamer-1.0`
Package gstreamer-1.0 was not found in the pkg-config search path.
Perhaps you should add the directory containing `gstreamer-1.0.pc'
to the PKG_CONFIG_PATH environment variable
No package 'gstreamer-1.0' found
basic-tutorial-1.c:1:21: fatal error: gst/gst.h: No such file or directory
 #include <gst/gst.h>
                     ^
compilation terminated.
santhosh@santhosh-Vostro-15-3568:~/Desktop/gstreamer$

advice how to resolve k

Regards

Santhosh

0 件の賞賛
返信
4 返答(返信)

6,487件の閲覧回数
vinaymanikkoth
Contributor II

Hi Santhosh,

I am also facing the same issue. were you able to solve this? if so can you guide me ? 

Thanks

Vinay

0 件の賞賛
返信

6,487件の閲覧回数
santhosh2
Contributor IV

Yes i was able to resolve it,

You need to add the gstreamer packages to yocto and generate the tool chain libraries. 

add the below configuration in local.conf file

CORE_IMAGE_EXTRA_INSTALL += "opkg apt packagegroup-fsl-gstreamer1.0-full imx-gst1.0-plugin gstreamer1.0 gstreamer1.0-plugins-ugly-meta packagegroup-fsl-gstreamer1.0-commercial gst-plugins-good-udp gst-variable-rtsp-server gstreamer1.0-plugins-base gstreamer1.0-plugins-good gstreamer1.0-plugins-bad gst-plugins-good-rtp gst-plugins-good-rtpmanager gst-plugins-good-rtsp gst-plugins-good-udp gst-plugins-good-matroska gst-plugins-base-videotestsrc gst-plugins-base-ffmpegcolorspace gst-fluendo-mpegdemux gst-plugins-base-ogg gst-openmax "

#RTSP Server dependency

LICENSE_FLAGS_WHITELIST += "commercial"
CORE_IMAGE_EXTRA_INSTALL += "gstreamer1.0-plugins-ugly gstreamer1.0-rtsp-server gtk-doc gst-plugins-good gst-plugins-bad gst-plugins-good gst-plugins-ugly"

Compile the yotoc using below command

bitbake fsl-image-validation-imx

bitbake fsl-image-validation-imx -c populate_sdk

After compilation of meta-toolchain, execute the below command to install the cross-compiler
$ sudo sh tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-fsl-image-validation-imx-aarch64-toolchain-4.14-sumo.sh

This should install the  tool-chain all required libraries to opt folder than you can export the tool chain path and should resolve your issue

Regards

Santhosh

6,487件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please use the Yocto BSP Linux L4.14.78_1.0.0 Documentation

0 件の賞賛
返信

6,229件の閲覧回数
darrenrobinson
Contributor I

we would if it would help resolve these kind of issues, but unfortunately it doesn't

0 件の賞賛
返信