How to compile mfgtool uboot under android 8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to compile mfgtool uboot under android 8.1

4,512 Views
hannywei
Contributor I

hi

I am using i.mx8m

After modifing uboot source code, I want to know how to  compile mfgtool uboot under android 8.1?

Labels (1)
0 Kudos
Reply
17 Replies

4,041 Views
传策薛
Contributor V

Have you solved this problem?

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

NO

0 Kudos
Reply

4,041 Views
传策薛
Contributor V

I sovled it,we should build another mfgtool uboot image,should change the uboot source,and there are some uboot errors we should fix it!

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

Can you share me the change and code?

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I am confiming it for you.

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

any update?

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

Have you confirmed it?

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

I have If the DDR is the same as our refrence board, you can directly use the default mfgtool. You do not need to build the mfgtool firmware. If you change the DDR you need to rebuild the firmware for your board mfgtool, About the mfgtool uboot here you can use the same one uboot image with your board uboot image.

Have a nice day

Rita

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

HI

The  DDR is same. 

Do you have a test? we have tried and failed.

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Here you can use the default mfgtool u-boot, and you need to copy your board images to the mfgtool file. Could you tell me your details steps?

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

The default mfgtool u-boot can not work.

sure ,I copy the board images to he mfgtool file , i following the guidance document.

the steps is the same as  i.MX8MQ u-boot和mgftool烧写emmc失败 

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can refer to our user guide document. And here could you tell me which flash you download the images to , EMMC or SD card?

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Here you can use the default mfgtool u-boot, and you need to copy your board images to the mfgtool file. Could you tell me your details steps?

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

Not success,my question is same as https://community.nxp.com/thread/479888 。

0 Kudos
Reply

4,041 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

About the mfgtool uboot here you can use the same one uboot image with your board uboot image. You do not need to compile special for it. You can have a try.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

hi Rita Wang

any update?

0 Kudos
Reply

4,041 Views
hannywei
Contributor I

Not success,my question is same as i.MX8MQ u-boot和mgftool烧写emmc失败 。

0 Kudos
Reply