How to compare read and write delay calibrations to pinpoint memory issue ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to compare read and write delay calibrations to pinpoint memory issue ?

1,474 Views
peteramond
Contributor V

Hi All,

In the document Freescale i.MX6 DRAM Port Application Guide – DDR3 we can see the sample read and write delay calibrations in section 3.1.2

From following write level calibration of  2 boards we can see from the red highlighted lines Board 1 has got 0x11111111 too early than Board 2. 

1) What can we figure from this ? If 0 represent pass values and 1 represent fail; according to user manual why some results are like 0x10111111 ?

2) If wider the 0 window, it represent more pass results for the ddr. Is that good or bad ?

3) Why it is showing at top and bottom half all 1 ? Is that mean read or write fails ? If at the very bottom result include 0 result what can we say about that byte lane ?

4) Can we get any failures of byte lane of the memory from this results ?

Regards,

Peter.

Board 1 (Working Board)

  1. ABS_OFFSET=0x00000000   result[00]=0x11111111
  2. ABS_OFFSET=0x04040404   result[01]=0x10111111
  3. ABS_OFFSET=0x08080808   result[02]=0x10110111
  4. ABS_OFFSET=0x0C0C0C0C   result[03]=0x10110010
  5. ABS_OFFSET=0x10101010   result[04]=0x10100010
  6. ABS_OFFSET=0x14141414   result[05]=0x00000000
  7. ABS_OFFSET=0x18181818   result[06]=0x00000000
  8. ABS_OFFSET=0x1C1C1C1C   result[07]=0x00000000
  9. ABS_OFFSET=0x20202020   result[08]=0x00000000
  10. ABS_OFFSET=0x24242424   result[09]=0x00000000
  11. ABS_OFFSET=0x28282828   result[0A]=0x00000000
  12. ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000
  13. ABS_OFFSET=0x30303030   result[0C]=0x00000000
  14. ABS_OFFSET=0x34343434   result[0D]=0x00000000
  15. ABS_OFFSET=0x38383838   result[0E]=0x00000000
  16. ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000
  17. ABS_OFFSET=0x40404040   result[10]=0x00000000
  18. ABS_OFFSET=0x44444444   result[11]=0x00000000
  19. ABS_OFFSET=0x48484848   result[12]=0x00000000
  20. ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000
  21. ABS_OFFSET=0x50505050   result[14]=0x00000000
  22. ABS_OFFSET=0x54545454   result[15]=0x00000000
  23. ABS_OFFSET=0x58585858   result[16]=0x00000000
  24. ABS_OFFSET=0x5C5C5C5C   result[17]=0x00000000
  25. ABS_OFFSET=0x60606060   result[18]=0x01000000
  26. ABS_OFFSET=0x64646464   result[19]=0x01000000
  27. ABS_OFFSET=0x68686868   result[1A]=0x01011110
  28. ABS_OFFSET=0x6C6C6C6C   result[1B]=0x01111111
  29. ABS_OFFSET=0x70707070   result[1C]=0x11111111
  30. ABS_OFFSET=0x74747474   result[1D]=0x11111111
  31. ABS_OFFSET=0x78787878   result[1E]=0x11111111
  32. ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111

Board 2 (Faulty board)

  1. ABS_OFFSET=0x00000000   result[00]=0x11111111
  2. ABS_OFFSET=0x04040404   result[01]=0x11111111
  3. ABS_OFFSET=0x08080808   result[02]=0x11110111
  4. ABS_OFFSET=0x0C0C0C0C   result[03]=0x10100010
  5. ABS_OFFSET=0x10101010   result[04]=0x10100010
  6. ABS_OFFSET=0x14141414   result[05]=0x10100000
  7. ABS_OFFSET=0x18181818   result[06]=0x00000000
  8. ABS_OFFSET=0x1C1C1C1C   result[07]=0x00000000
  9. ABS_OFFSET=0x20202020   result[08]=0x00000000
  10. ABS_OFFSET=0x24242424   result[09]=0x00000000
  11. ABS_OFFSET=0x28282828   result[0A]=0x00000000
  12. ABS_OFFSET=0x2C2C2C2C   result[0B]=0x00000000
  13. ABS_OFFSET=0x30303030   result[0C]=0x00000000
  14. ABS_OFFSET=0x34343434   result[0D]=0x00000000
  15. ABS_OFFSET=0x38383838   result[0E]=0x00000000
  16. ABS_OFFSET=0x3C3C3C3C   result[0F]=0x00000000
  17. ABS_OFFSET=0x40404040   result[10]=0x00000000
  18. ABS_OFFSET=0x44444444   result[11]=0x00000000
  19. ABS_OFFSET=0x48484848   result[12]=0x00000000
  20. ABS_OFFSET=0x4C4C4C4C   result[13]=0x00000000
  21. ABS_OFFSET=0x50505050   result[14]=0x00000000
  22. ABS_OFFSET=0x54545454   result[15]=0x00000000
  23. ABS_OFFSET=0x58585858   result[16]=0x00000000
  24. ABS_OFFSET=0x5C5C5C5C   result[17]=0x00000000
  25. ABS_OFFSET=0x60606060   result[18]=0x00000000
  26. ABS_OFFSET=0x64646464   result[19]=0x00000000
  27. ABS_OFFSET=0x68686868   result[1A]=0x00000000
  28. ABS_OFFSET=0x6C6C6C6C   result[1B]=0x01001000
  29. ABS_OFFSET=0x70707070   result[1C]=0x01001111
  30. ABS_OFFSET=0x74747474   result[1D]=0x01111111
  31. ABS_OFFSET=0x78787878   result[1E]=0x01111111
  32. ABS_OFFSET=0x7C7C7C7C   result[1F]=0x11111111
Labels (5)
1 Reply

1,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

results 0x10111111 are high and low failure points as described in

sect.13 Read DQS Delay Calibration AN4467 i.MX6 Series DDR Calibration

https://www.nxp.com/docs/en/application-note/AN4467.pdf 

>2) If wider the 0 window, it represent more pass results for the ddr. Is that good or bad ?

good

>4) Can we get any failures of byte lane of the memory from this results ?

these results seem as good, so from them there is no way to tell reason for linux failures.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------