Hi everyone! i am doing a project in CAN network communication. In this, I am using IMX 6 controller as the master and PIC 18F458 as the slave. I want them to communicate in either 125 Kbps or 500 Kbps. I programmed the PIC controller with a baud rate of 125 Kbps. But while giving linux commands after interfacing both PIC and IMX controllers, I didnt receive any message to the receiver (i.e) PIC. Rather, when i typed a command as ifconfig can0, i am getting as RX packets:2 and TX packets:0. Actually my doubt is that how the IMX controller will receive as it is the transmitter here. Moreover, I am a beginner in linux. Please guide me as I got stucked in this area.
Thanks & Regards,
Harishankari