How to check whether i.MX6Q GPU acceleration is valid.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check whether i.MX6Q GPU acceleration is valid.

ソリューションへジャンプ
1,994件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6Q GPU.

I consider using Qt GUI with Linux system.

Then, I want to check whether CPU acceleration is valid or not for drawing Qt GUI.

Could you let me know how to check it?

Actually, I came up with two methods as below, but I cannot judge to "GPU acceleration is valid" with both methods.

----------

1. Check whether OpenGL ES libraries (e.g. ligGAL.so, libEGL.so, libVIVANTE.so, etc...) are loaded when Qt process is running.

I can understand what libraries is loaded, but cannot conclude to "GPU acceleration is valid".

2. Check CPU load by top command when GPU sample program (gpu_sdk_v1.00.tar.gz) is running.

I can guess "maybe, GPU acceleration is valid because CPU load is low", but cannot conclude.

----------

Best Regards,

Satoshi Shimoda

ラベル(4)
タグ(2)
1 解決策
1,153件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, it should be accelerated by GPU, in order to see how much (in numbers) is accelerated, you can check it with the vProfiler tool,

If you already have the GPU_SDK, please check the Documentation folder, in order to use the profiler, if not You can download the vivante tools from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

More info:

https://community.freescale.com/docs/DOC-94066

https://community.freescale.com/message/348829

https://community.freescale.com/message/359691

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,154件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Yes, it should be accelerated by GPU, in order to see how much (in numbers) is accelerated, you can check it with the vProfiler tool,

If you already have the GPU_SDK, please check the Documentation folder, in order to use the profiler, if not You can download the vivante tools from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

More info:

https://community.freescale.com/docs/DOC-94066

https://community.freescale.com/message/348829

https://community.freescale.com/message/359691

Regards

0 件の賞賛
返信