How to check REV version

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to check REV version

3,129 次查看
harekrishnaroy
Contributor III

Hi All,

I am using i.Mx6Q sabreauto . I want to check REV version of it. Re: PCIE link up failed when booting the kernel on IMX6QSD board    suggest that if i want to use pcie then i have to use REV C or later board. how would i check this?

标签 (1)
5 回复数

2,788 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hare

please check board marking SCH-xxxxx REV

1.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,788 次查看
harekrishnaroy
Contributor III

Hi igorpadykov ,

     I checked board and found  700-27142-REVX4  & SCH-27142-REV B1 . May be i am using older version board.  But i have another board with 700-27142-REV A & SCH-27142-REV C.  Will this board support pcie.

REV A in "700-27142-REV A" is cofusing !!

Regards ,

Hare Krishna

0 项奖励
回复

2,788 次查看
igorpadykov
NXP Employee
NXP Employee

"700-27142-REV A" is assembly revision, not board revision.

Best regards

igor

2,788 次查看
harekrishnaroy
Contributor III

Hi igor ,

                  Thank you very much for your quick responce. I am trying to enable pcie. I am trying this on i.Mx6Q sabreauto with SCH-27142-REV C.

As i have browsed on forum and found that this board should support pcie.  But i am getting following error!!

iMX6 PCIe PCIe RC mode imx_pcie_pltfm_probe entering.

PCIE: imx_pcie_pltfm_probe start link up.

link up failed, DB_R0:0x001f3e00, DB_R1:0x08200000!

IMX PCIe port: link down!

I have used L3.0.35_4.1.0_130816_source.tar.gz. pcie device is of Atheros. 

what could be the possible reason for this issue?

Regards ,

Hare Krishna

0 项奖励
回复

2,788 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hare

please create new thread for this problem.

Best regards

igor

0 项奖励
回复