How to change to ldo bypass mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change to ldo bypass mode?

ソリューションへジャンプ
2,313件の閲覧回数
kris_fei
Contributor III

Platform: IMX6DL
OS: Android 4.4
Kernel branch: 3.0.35

The temperature of our board is too high, i want to change to ldo bypass mode to low its temperature, 

how to configure it by software?

ラベル(1)
1 解決策
2,011件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,012件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,011件の閲覧回数
kris_fei
Contributor III

thanks, found it ~

0 件の賞賛
返信