How to change to ldo bypass mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change to ldo bypass mode?

跳至解决方案
2,368 次查看
kris_fei
Contributor III

Platform: IMX6DL
OS: Android 4.4
Kernel branch: 3.0.35

The temperature of our board is too high, i want to change to ldo bypass mode to low its temperature, 

how to configure it by software?

标签 (1)
1 解答
2,066 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
2,067 次查看
igorpadykov
NXP Employee
NXP Employee

Hi

please refer to attached Release Notes

Table 6. Kernel Boot Parameters, parameter "ldo_active".

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,066 次查看
kris_fei
Contributor III

thanks, found it ~

0 项奖励
回复