How to change the drive strength of MIPI-DSI output in i.MX7D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the drive strength of MIPI-DSI output in i.MX7D

跳至解决方案
2,941 次查看
ko-hey
Senior Contributor II

Hi all

Are there any registers to change the drive strength of MIPI-DSI in i.MX7D ?

I'm on the compliance test of MIPI-DSI with custom board.

It failed in the section of Rise time in HS mode.

It's too slow both rise time and fall time.

So if there are registers to modify the drive strength, I want to try it.

Are there any registers to change the drive strength of MIPI-DSI in i.MX7D ?

If there are no registers to modify it, please advice me to improve the rise time.

Ko-hey

标签 (3)
0 项奖励
回复
1 解答
2,548 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi ko-hey,

you are right, I checked and MIPI pins are dedicated to this module, so they are not multiplexed with other functionalities and they are not configurable, however our modules are compliant with the specs. You may need to check your hardware to verify why you are facing such latency.

Sorry for the inconvenience.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,548 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi ko-hey,

Please see Drive Strength Field (DSE) in IOMUXC_LPSR_SW_PAD_CTL_PAD_GPIOx_IOxx register on chapter 8 IO and Pinmux
of Reference Manual http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX7DRM.pdf 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,548 次查看
ko-hey
Senior Contributor II

Hi

I think the register which you mentioned is for MUX pin such as BOOT_MODE0.

ex) DSE field of IOMUXC_LPSR_SW_PAD_CTL_PAD_BOOT_MODE0 register

I talked about following fixed pins.

MIPI_DSI_CLK_P/N

MIPI_DSI_D0_P/N

MIPI_DSI_D1_P/N

Do you have register to control the pins ?

Ko-hey

0 项奖励
回复
2,549 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi ko-hey,

you are right, I checked and MIPI pins are dedicated to this module, so they are not multiplexed with other functionalities and they are not configurable, however our modules are compliant with the specs. You may need to check your hardware to verify why you are facing such latency.

Sorry for the inconvenience.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,548 次查看
ko-hey
Senior Contributor II

Hi

Could you advise me which part do we check in hardware ?

Ko-hey

0 项奖励
回复
2,548 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi ko-hey,

If rise time and fall time are too slow most likely the problem is layout. There are some things you can verify:

- shorten distance between sensor and i.mx
- verify that the camera power source is not affecting other devices and add a bypass capacitor
- you can also check that all the wires of the camera connector are properly connected and double check any posibilty of intermittent open pins


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------