How to change the default Camera

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the default Camera

1,252件の閲覧回数
phillipchen
Contributor I

I have two EVBs, which are MCiMX6Q-SDP and MCiMX6Q-SDB. I installed the camera, which comes from the MCiMX6Q-SDP, on the front camera port (J9)of the MCiMX6Q-SDB. Because the default camera is the rear camera (J5), I still can't start the camera function after I installed the camera on the MCiMX6Q-SDB. How can I change the default camera?

Thanks

Best Regards,

Phillip

ラベル(2)
0 件の賞賛
返信
0 返答(返信)