How to change ddr3 frequency from 528M to 400M for imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to change ddr3 frequency from 528M to 400M for imx6q

1,083 次查看
pengxingwei
Contributor III

hello,

            my board was designed accroding IMX6Q SABRESD, on which the OS is Android4.4.2 and u-boot 2009.08-dirty,now I want to change the ddr3 frequency from 528M to 400M,I want how to do for it ? the relative file is generic. Thanks

Original Attachment has been moved to: generic.c.zip

标签 (2)
0 项奖励
回复
2 回复数

938 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  I hope the following helps

linux-2.6-imx.git - Freescale i.MX Linux Tree 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

938 次查看
pengxingwei
Contributor III

hello,

            Thanks your reply ! don't understand why to care for the kernel file?  Don't  just change the uboot file if I want to change the ddr frequency?

0 项奖励
回复