How to change bootloader(u-boot) splash screen/logo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change bootloader(u-boot) splash screen/logo

ソリューションへジャンプ
10,395件の閲覧回数
ajaisingh
Contributor II

Hi Everybody

         I have MCIMX6Q-SDP sabre board,I am booting android from sd card. I need to change u-boot bootloader splash screen/logo while the system start up.

        Can anybody please suggest me some ways to change bootloader splash screen/logo in the android source code.

  Thank you all in advance.

With Regards

Ajai Singh

タグ(2)
0 件の賞賛
返信
1 解決策
4,734件の閲覧回数
winstonrodrigue
Contributor IV

Dear Ajai Singh,

    you could also refer the document uboot_mx5x.pdf which is in 11.09 documentation bundle.

please refer to section 5.5 Splash Screen Support.  then u can get the splash screen.

Winston.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,735件の閲覧回数
winstonrodrigue
Contributor IV

Dear Ajai Singh,

    you could also refer the document uboot_mx5x.pdf which is in 11.09 documentation bundle.

please refer to section 5.5 Splash Screen Support.  then u can get the splash screen.

Winston.

0 件の賞賛
返信
4,734件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please take a look at the following :

https://community.freescale.com/message/319620#319620

0 件の賞賛
返信
4,734件の閲覧回数
ajaisingh
Contributor II

Thanks Yuri for your reply,but i need to change the boot-loader logo when we power up the board and not the android system boot up logo.

Please suggest me if some ways are available for this.

Thank You

0 件の賞賛
返信