How to burn OTP bits for iMX28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to burn OTP bits for iMX28

1,334 Views
liuxing
Contributor II

Hi All,

   I want to confirm that the Freescale Manufacturing Tool means the mfg tool?

  If so,I can't find the difference between the os image and OtpInit.sb.Is the difference in ucl.xml file?

  Can you provide the ucl.xml example for burning OTP bits?

8.1.4. Burn the OTP bits
Use the Freescale Manufacturing Tool to burn OTP bits before updating the
device's firmware. The Manufacturing Tool looks for OtpInit.sb in its firmware
profile, so copy or move the OtpInit.sb file to the firmware folder under the
Manufacturing Tool's profile.

Labels (1)
0 Kudos
Reply
1 Reply

1,306 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, it mean mfgtool.The OTP area access feature is NOT implemented in GPMI NAND driver in any of our BSP releases.For this Micron part, the OTP data read & program is similar to typical page read & page program but using different command sequence. The customer can refer to  GPMI NAND driver and add code to validate the OTP area program, protect and read function.

I found the following threads hope can do help for you.

How to enable SPI NOR boot for i.MX28 (Spansion s25fl256s) 

HAB i.MX28 Invalid Certificate 

0 Kudos
Reply