How to build imx-boot image file for i.MX8M Mini ECSPI?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build imx-boot image file for i.MX8M Mini ECSPI?

ソリューションへジャンプ
4,763件の閲覧回数
m_c
Senior Contributor I

Since the image vector table offset is different of FlexSPI (QSPI) and ECSPI.

How to build imx-boot image for ECSPI like imx-boot-imx8mmevk-fspi.bin-flash_evk_flexspi for QSPI by Linux yocto BSP?

pastedImage_6.png

pastedImage_9.png

ラベル(1)
0 件の賞賛
返信
1 解決策
4,129件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

one can build in the same way as emmc (also 0x400 offset), use

sect.4.5.12 How to build U-Boot, sect.4.5.13 How to build imx-boot

attached Linux Guide. Other useful tutorial:

https://developer.solid-run.com/knowledge-base/i-mx8m-atf-u-boot-and-linux-kernel/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
4,130件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi m.c.

one can build in the same way as emmc (also 0x400 offset), use

sect.4.5.12 How to build U-Boot, sect.4.5.13 How to build imx-boot

attached Linux Guide. Other useful tutorial:

https://developer.solid-run.com/knowledge-base/i-mx8m-atf-u-boot-and-linux-kernel/ 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信