How to build/generate imx-boot-imx8qxpmek-sd.bin-flash binary for imx8qxp mek

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to build/generate imx-boot-imx8qxpmek-sd.bin-flash binary for imx8qxp mek

2,926 次查看
jordonwu
Contributor III

According i.MX_Yocto_Project_User's_Guide.pdf of L4.14.98_2.3.0, we have success build yocto bsp using below cmd:

$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m imx-4.14.98-2.3.0.xml

$ DISTRO=fsl-imx-xwayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-wayland

$ bitbake core-image-minial

on build-xwayland\tmp\deploy\images\imx8qxpmek directory, we can found below files:

imx-boot-imx8qxpmek-sd.bin

imx-boot-imx8qxpmek-sd.bin-flash_linux_m4

imx-boot-imx8qxpmek-sd.bin-flash_spl

But can't found imx-boot-imx8qxpmek-sd.bin-flash (with suffix -flash), I checked L4.14.98_2.3.0_images_MX8QXPMEK.zip , which contains imx-boot-imx8qxpmek-sd.bin-flash , and this file is used for uuu flash tool.

So my question is: on yocto bsp (such as 4.14.98_2.3.0 branch), how to build/generate imx-boot-imx8qxpmek-sd.bin-flash file? Thanks.

0 项奖励
回复
4 回复数

2,787 次查看
jordonwu
Contributor III

Any update for this question? thanks

0 项奖励
回复

2,748 次查看
fei_4_xu
Contributor III
0 项奖励
回复

2,787 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Use the one you build, in the uuu script replace the imx-boot-imx8qxpmek-sd.bin-flash use the one imx-boot-imx8qxpmek-sd.bin you build.

0 项奖励
回复

2,787 次查看
jordonwu
Contributor III

@Rita Wang,

Thanks, I will try it.

0 项奖励
回复